{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.

What is the DC breaking capacity for MCB of type iC60H ?

The MCB of type iC60H has DC breaking capacity as Follows:

- 1 pole: 10 KA - for Voltage up to 72 V DC.
- 2 poles: 10 KA for Voltage from 100 to 133 V DC
- 3 poles: 10 KA for Voltage from 100 to 133 V DC
- 4 Poles: 10 KA for voltage from 220 to 250 V DC.

attached data sheet for the MCB of type iC60H

Schneider Electric Egypt and North East Africa

Attachment(s)

iC60H.pdfiC60H.pdf [542.95 KB]