{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What are the Differences between Motor Circuit Breakers of types GV2ME and GV2RT ?

Both GV2ME and GV2RT are Thermal Magnetic Motor Circuit breakers (that don't need external Thermal overload relay),

The Main Differences are found in the following points:

- GV2ME:
- Control is done by Push buttons
- It is used with Motors with motors of normal applications

- GV2RT:
- Control of the CB is by Rocker Lever
- It is used Mainly with special motors of high Peak Current on starting rather than normal applications

Schneider Electric Egypt and North East Africa