{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.

What is the difference between Class 10 and class 20 Overload Relays For Thermal overload relays ?

- For all types of thermal overload relays (LRD or LR9D or LR9F), These can be classified as follows:
* Class 10: According to IEC60947-4-1, it specifies the tripping time for 7.2 In to be between 2 to 10 Seconds
* Class 20: According to IEC60947-4-1, it specifies the tripping time for 7.2 In to be between 6 to 20 Seconds

This difference in tripping time has value in time coordination,

Schneider Electric Egypt and North East Africa