Search FAQs
RS-485 Converters for the UPS SmartSlot Building Management Card (AP9622)
Issue
RS-485 Converter Compatibility for AP9622 Building Management Modbus/JBUS UPS SmartSlot card
Product Line
- UPS Device Management
- AP9622 Building Management Modbus/JBUS UPS SmartSlot Card
Environment
AP9622 installations requiring RS-232 to RS-485 converter to work with various Building Management Systems
Cause
The AP9622 card supports RS-232 Modbus/JBUS output. Users may require RS-485 adapters to work with an existing Building Management System. Refer to compatibility list below.
Resolution
The Building Management Integration Card (AP9622) will work with the following RS-232 to RS-485 converters:
- B&B Electronics P/N: 485OT9L*
*Item is currently discontinued per B&B. The recommended replacement is 4WSD9OTB but it has not been tested with the AP9622.
- B&B Electronics P/N: 485LP9TB
Below is an example diagram for a 485LP9TB application:
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: