Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
What are the pinouts for the Output Relay on the Environmental Monitoring Unit (AP9319) and the Environmental Management System (AP9320)?


Below are the pinouts:


 

Pin #

 Description

 1

 No Connection

 2, 3

 Normally Closed (NC) Contact

 4, 5

 Common

 6, 7

 Normally Open (NO) Contact (recommended connection)

 8

 No Connection


Relay ratings: 1A, 30V AC/DC



Since the user interface allows for either 'normally open' or 'normally closed,' APC recommends using only the normally open contacts and configuring the 'normal' state in the user interface.



 

Schneider Electric Egypt and North East Africa

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category: