{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can I connect a Macintosh computer to my Analog KVM Switch (AP5201/AP5202)?


Issue

Can I connect a Macintosh computer to my Analog KVM Switch?


Product Line
  • Rack Accessories - KVM Switches
    • AP5201
    • AP5202

Environment
  • All serial numbers
  • All firmware versions
  • Mac OS X or higher

Cause

APC does not sell a KVM cable that connects direct from the AP5201/AP5202 KVM switch to a Macintosh computer.


Resolution

APC engineering has tested use of part number 19044 (PS/2 to USB adapter) to be used in conjunction with the AP5201/AP5202 KVM switch. The 19044 connects to the PS/2 connection on your KVM cable. The USB adapter then connects to your Macintosh computer.

APC engineering only tested this configuration with Macintosh computers running version OSX 10 or higher. Operating systems previous to 10 are not tested and proved to work.


Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: