Issue
Does pressing the pinhole reset button on a Metered or Switched Rack PDU or Rack ATS cause the outlets to reboot or disrupt power in any way?
Product Line
- Rack Power Distribution - Power Distribution Units and Automatic Transfer Switch
- AP77XX - Rack ATS
- AP44XX - Rack ATS
- AP78XX - Metered Rack PDU
- AP79XX - Switched Rack PDU
- AP84XX - Metered By Outlet PDU
- AP86XX - Switched Rack PDU with Metering By Outlet
- AP88XX - Metered Rack PDU 2G
- AP89XX - Switched Rack PDU 2G
Environment
- All installations
Cause
Many users ask if rebooting their network management card affects outlet status or power output of their device. See below for additional information.
Resolution
Resetting the network interface using the small reset button near the network jack has no effect on the electrical output of the Rack PDU or Rack ATS. This procedure simply reboots the embedded Network Management Card, which will render the network port inaccessible for a short period of time while it reboots.
Released for: Schneider Electric Egypt and North East Africa