Issue
SNMPv3 is not working properly with my Network Management Card (possibly v3.5.7 or below).
Product Line
- Network Management Card 1 (NMC1) - AP9617, AP9618, AP9619
Devices with an embedded Network Management Card 1 include (but are not limited to): Metered/Switched Rack PDUs (AP78XX, AP79XX), Rack Automatic Transfer Switches (AP77XX, Environmental Monitoring Units (AP9320, AP9340, Netbotz 200)
Environment
- All serial numbers
- NMC1 versions v3.5.7 and below
Cause
In some cases, you may find that one more of the SNMPv3 profiles “timeout” or have communication issues with Network Management Card 1 (AP9617, AP9618, AP9619 and any device with an embedded version of this card). In such cases, APC has found resetting the card to defaults fixes this issue.
Resolution
AOS versions > v3.5.8 contain the firmware fix for this issue. Please seek an upgrade if you are experiencing these symptoms.
The steps below only need to be performed as a workaround to the issue if you have AOS 3.5.7 or lower or cannot update.
- Login to the NMC Web Interface via the IP address with the correct username/password.
- Select the following to Reset the NMC to defaults without losing your network configuration
- Administration Tab
- General menu selection on the horizontal menu bar
- Reset/Reboot menu selection on the Vertical menu bar
- Select the Reset All Radio Button
- Put a check in the Exclude TCP/IP checkbox
- Select the Apply button to start the Reset to Defaults process.
- Select the Apply button to confirm the Reset/Reboot Management Interface Confirmation process.
- Select the following to Reboot the NMC
- Administration Tab
- General menu selection on the horizontal menu bar
- Reset/Reboot menu selection on the Vertical menu bar
- Select the Reboot Management Interface Radio button
- Select the Apply button to start the Reboot Management Interface process.
- Select the Apply button to confirm the Reset/Reboot Management Interface Confirmation process.
- Select the following to setup the SNMPv3 support in the NMC:
- Administration Tab
- Network menu selection on the horizontal menu bar
- Select the SNMPv3 "User Profiles" menu in the Vertical menu bar of the NMC to setup each SNMPv3 User Profile.
- Select the user profile that you want to modify
- Modify the User Name in the user input field provided.
- Modify the Authentication Passphrase in the user input field provided if you plan on using MD-5 Authentication with the SNMPv3 data. NOTE: The password must be 15-32 ASCII characters long.
- Modify the Privacy Passphrase in the user input field provided if you plan on using DES encryption with the SNMPv3 data. NOTE: The password must be 15-32 ASCII characters long.
- Select the MD-5 radio button in the Authentication Protocol row if you plan on using MD- Authentication with the SNMPv3 data.
- Select the DES radio button in the Privacy Protocol row if you plan on using DES encryption with the SNMPv3 data.
- Select the Apply button to enable your changes for each profile.
- Complete steps i - vi for each profile that you want to create up to a maximum of four.
- Select the SNMPv3 "Access Control" menu in the vertical menu bar of the NMC to setup access control for each of the SNMPv3 User Profiles
- Select the user profile that you want to give access control to
- Select the Enable checkbox to enable SNMPv3 control to a user profile.
- Select the User Name of the user profile that you want to enable
- Select the NMS IP/Hostname IP Address of the system that will be used to communicate via SNMPv3 to this NMC. NOTE: 0.0.0.0 indicates all systems can interface via SNMPv3 to the NMC as long as the system user profile, authentication passphrases, and encryption passphrases match the NMC.
- Select the Apply button to enable the changesSelect the SNMPv3 "access" menu in the vertical menu bar of the NMC to enable SNMPv3 for the NMC.
- Select the Enable SNMPv3 access checkbox.
- Select the Apply button to enable SNMPv3 for the NMC.
NOTE: The NMC requires that the user logout of the NMC and it will automatically reboot after logout to institute these changes. Upon rebooting, the NMC will take about 5-10 minutes to complete its backend processes needed in order to enable SNMPv3. Upon accessing the web interface during this 5-10 minute period, until this process is complete, the NMC will display a message saying "Please wait while system is booting..." but telnet access will still be available.
Released for: Schneider Electric Egypt and North East Africa