{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

AP8XXX Series Rack PDU Power Output Specifications (CAN & USB ports)


Issue

This article will review the power output capabilities for the CAN and USB ports on an AP8XXX series Rack PDU.


Product Line

  • Rack Power Distribution (PDU) Models
    • AP84XX
    • AP88XX
    • AP89XX
    • AP86XX


Environment

  • All serial numbers
  • All firmware versions


Cause

Information is provided for reference only.


Resolution


Below is a diagram of the current AP8XXX series Rack PDU display for reference:
















Item NumberDescriptionMaximum Output Power
7CAN Bus Ports (for Network Port Sharing use only)200mA @ 24VDC nominal (4.8 watts)
8USB Port - (for USB drive to upgrade PDU firmware only)100mA @ 5VDC nominal












Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: