Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
NEMA 5-15 receptacle description

Article available in these languages: Spanish

Issue:
Which terminal is which in a standard household outlet?    

Cause:
Informational

Resolution:
The NEMA 5-15 receptacle is the most common electrical receptacle in the United States and Canada. It is a two-pole, three-wire grounding receptacle which is used for a maximum of 15A and 125V. The standard wire colors are green for Ground and white for Neutral. The color of the Hot wire can vary depending on the building's electrical scheme; most common colors for the Hot wire are black and red. The individual prongs: Hot, Neutral & Ground are well differentiated as indicated in the diagram below.
NEMA 5-15 power outlet

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range: