Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Symmetra PX1-PX2; What happens when PX1, PX2 and 250/500K PX is EPO'd
Issue:
What happens when PX1, PX2 and 250/500K PX is EPO'd
Product line:
Symmetra PX
Environment:
All models, all serial numbers
Cause:
This document describes how the Symmetra PX reacts to the EPO circuit being activated. Emergency Power Off (EPO) is the capability to power down a piece of electronic equipment or an entire installation, in the case of an emergency, from a single point by activating a push button.
For 20K, 40K, 80K PX:
If the EPO circuit in the Symmetra PX is activated the System Enable Switch turns to the off position, the DC Breaker in the Main Frame or in the XR Frame (80kw units only) will trip. Mains feed CB will be tripped on ISX PDU. There is no power on the output of the XR Battery Frames or on the output of the Symmetra PX UPS.
An EPO event is not recorded in the Event Log.
For 100K PX:
Only the Battery CBs on XR frames will be tripped. Customer would need to have optional shut trip on Upstream CB to turn off input power to UPS.
For 250K/500K PX:
All Battery CBs on battery frames and Q2 will be tripped
Resolution:
Reset EPO switch and follow proper procedures to restart UPS
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: