{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.

88 volts from the North American Symmetra Power Array output block

Issue
88 volts is measured between a conductor and ground/neutral from the North American Symmetra Power Array output block

Product Line
Symmetra Power Array

Environment
North American models only (SYMSTRF or SYMINIF)

Cause
The design of the isolation transformer in the North American Symmetra Power Array allows multiple output voltages to be derived. The output terminal block provides two 120 volt legs and one 88 volt leg. Once the needed output voltage is determined it is imperative to validate the appropriate legs to take to the panel to generate the needed output voltage. The 88 Volt leg is used with the 120 volt leg to derive 208 volts as needed for 208 volt loads.

The taps on the block are listed below :

  • Tap 2 generates 120 Volts
  • Tap 4 generates 88 volts
  • Tap 6 generates 120 Volts

For more information, please reference page 4-4 of the Symmetra Power Array user manual .


Resolution
No resolution is necessary.  This is normal operation.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: