Search FAQs
Symmetra LX shows site wiring fault and/or has clicking power modules
Issue
Symmetra LX runs on battery and may exhibit audible clicking from the power modules. Erroneous messages regarding output voltage may also occur. If the SYMIM5 firmware is rev 512 or above, the UPS may show "Site Wiring Fault."
Product Line
Symmetra LX
Environment
All serial ranges
Cause
A neutral wire is needed in order for the Symmetra LX to operate online correctly. A missing neutral or a neutral that is not properly bonded to ground at the upstream panel or transformer can cause the UPS to exhibit the symptoms above.
Resolution
If these symptoms are present, an input wiring check should be completed to ensure a neutral is being fed to the UPS and is connected to the correct terminal. The neutral must be properly bonded to ground. Without one, the Symmetra LX will not operate properly.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: