{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Single Phase Symmetra Installation Clearances



Issue

What are the recommended front and rear clearances for the installation of a single phase Symmetra UPS system that is in tower form factor?



Product Line

Symmetra LX
Symmetra Power Array



Environment

All serial ranges



Cause

To ensure proper airflow and access for maintenance, Symmetra LX should be installed with the proper front and rear clearances.



Resolution

The recommended front clearance is 48" and the recommended rear clearance is 12".  There is no recommendation for side clearance as long as there is access to the front and rear of the system for maintenance.



Schneider Electric Egypt and North East Africa