Search FAQs
Are there spare or replacement keys available for the NetShelter SX, SV or VX cabinets?
Issue:
Customers require spare keys for their cabinets?
Customers require spare keys for their cabinets?
Product Line:
NetShelter SX, NetShelter SV, NetShelter VX
NetShelter SX, NetShelter SV, NetShelter VX
Environment:
All models and serial ranges.
All models and serial ranges.
Cause:
Keys can be lost, or extras may be needed.
Keys can be lost, or extras may be needed.
Resolution : Yes, a spare key can be purchased using Part number W870-8135. This is a single spare key which works on the NetShelter SX, SV and VX doors and side panels.
It also works on the NetShelter WX models AR106, AR109 and AR112.
It also works on the NetShelter WX models AR106, AR109 and AR112.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: