{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can split doors be installed on the front of a NetShelter SX, VX or SV cabinet?
Issue:
It can not be assumed that the rear split doors will install onto the front of the cabinet. Confirmation is needed.

Product Line:
NetShelter SX, NetShelter VX, NetShelter SV
Environment:
All versions and serial ranges.
Cause:
A customer may want to install split doors onto the front of a NetShelter SX cabinet.
Resolution :

Rear split doors can be installed onto the front of a NetShelter SX, VX and SV cabinets.
A replacement split door kit can be purchased or the existing split rear doors can be swapped to the front of the cabinet.
The replacement door kit includes all of the necessary hardware, including hinges.
The NetShelter one-piece front door may also be installed onto the rear of the cabinet.

Schneider Electric Egypt and North East Africa