{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is there a roof available for the AR3100 which is solid and does not have open cable access holes?
Issue:
There may be a need for a solid roof on the cabinets.

Product Line:
NetShelter SX

Environment:
All versions and serial ranges.

Cause:
A more secure roof may be required for installations such as PCI.

Resolution:
The WAR7210 can be used where high security is required. It is compatible with the following models: AR3100, AR3104, AR3105, AR3200 and AR3107.
For more information and a photo please see the attached file.

Schneider Electric Egypt and North East Africa

Attachment(s)
20131206 WAR7210 High Security Roof.pdf [20.32 KB]