{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How much exhaust clearance is needed for a NetShelter CX cabinet?

Issue:
The NetShelter CX may overheat if there is not proper clearance for airflow.
Product Line:
NetShelter CX
Environment:
All models and serial ranges.
Cause:
Improper spacing can cause overheating.
Resolution :
See attached file.
NetShelter CX Wall Clearance
The exhaust fans of the NetShelter CX vent to the sides. The back of the cabinet can be placed against a wall if desired.
If the cabinet is being installed in a corner please leave at least 6 inches of open space between the side of the NetShelter CX and the wall.
It is not recommended to install a NetShelter S X where the back and both sides are against a wall.
Please see attached file for a graphic depiction of the clearance.

Schneider Electric Egypt and North East Africa

Attachment(s)

NetShelter CX Exhaust Clearance Rev 20120402.pdfNetShelter CX Exhaust Clearance Rev 20120402.pdf [49.28 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: