Search FAQs
Where are the Model and Serial numbers on the NetShelter SX, SV or VX?
Issue:
Customer cannot find the serial number of the NetShelter cabinet.
Product Line:
NetShelter
Environment:
All versions and serial ranges.
Customer cannot find the serial number of the NetShelter cabinet.
Product Line:
NetShelter
Environment:
All versions and serial ranges.
Cause:
Need to locate the serial number.
Need to locate the serial number.
Resolution:
The serial number and model number are located on a label inside the rear doors on the top of the frame. Simply open the rear doors and look up.
See attached file for photos.
The serial number and model number are located on a label inside the rear doors on the top of the frame. Simply open the rear doors and look up.
See attached file for photos.
Released for:Schneider Electric Egypt and North East Africa
Attachment(s)
Explore more
Range:
Explore more
Range: