{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What's the difference between shipping load, dynamic load and static load? Which standards are used to certify these ratings?
Issue:
Shipping, moving and loading cabinets requires the installer to know the difference between shipping load, dynamic load and static load ratings.

Product Line:
NetShelter SX

Environment:
All versions and serial ranges.

Cause:
Installers and designers need to make sure the load capacity of the cabinet is not exceeded during installation, travel or operation.

Resolution:

Please see attachment for load ratings, definitions and standards.

Schneider Electric Egypt and North East Africa

Attachment(s)
20120330 NetShelter SX Load Rating Information Rev 7.pdf [219.69 KB]