Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
Computers containing PFC (Power Factor Corrected) power supplies and their use with Back-UPS and Smart-UPS SC with Step Approximated Sine waves.

Article available in these languages: Spanish

Issue:

Power Factor Corrected (PFC) power supplies are becoming increasingly popular in desktop PC’s in North America. Contributing to this trend is the fact that Energy Star 4.0 compliance as of July 2007, requires the use of PFC in desktop PC’s.

Please see reference to the Energy Star 4.0 compliance Tier 1 at www.energystar.gov/


Product Line:

Back-UPS CS, Back-UPS ES "U", Back-UPS ES "R", Back-UPS ES "G" (prior to 2013),
BX/BR1000 "G" (prior to 2013), BX/BR Families, Smart UPS SC

Environment:

Back-UPS CS, Back-UPS ES "U", Back-UPS ES "R", Back-UPS ES "G" (prior to 2013),
BX/BR1000 "G" (prior to 2013), BX/BR Families and Smart UPS SC


Cause:

What is Power Factor and Power Factor Correction?
Power factor is the percentage of electricity that is being used to do useful work. It is expressed as a ratio. For example, a power factor of 0.72 would mean only 72% of your power was being used to do useful work. Perfect power factor (which in this case is being achieved by the computer’s PFC power supply) is 1.0 (unity), meaning 100% of the power is being used for useful work. Power Factor Correction is a circuit design technique to increase the power factor of a device so that it approaches 1, or unity power factor.

Although computer power supplies draw only a fraction of their full capacity during it’s steady state(normal operation), PFC power supplies have the potential to draw their full capability during initial inrush. ""Inrush"" or ""Inrush Current"" refers to the maximum instantaneous input current drawn by an electrical device when first turned on.


Resolution:

A computer’s power supply may also be subjected to a period of inrush, while the UPS is changing state (switching from utility power to battery power and back). Back-UPS and Smart-UPS SCs may experience up to an 8ms transfer time during this period. This is just long enough to remove power from the PFC power supply, resulting in a momentary inrush of the PFC. Once the UPS changes states from ""Online"" (passing utility power) to ""On battery"" (passing power from the UPS's internal battery), the momentary inrush from the attached equipment subjects the UPS to the On battery power supply’s maximum power draw, resulting in a potential Overload condition or dropped load.

An Energy Star 4.0 compliant power supply has to be more than 80% efficient. For example, if a attached power supply is delivering 600W output power, its ‘input’ power can be as high as 750W. .

This ‘input’ power should be the basis for sizing the UPS, so as not to Overload the UPS. This can be calculated by taking the PFC power supply’s rated output power and multiplying it by 1.25 as follows;

600W x 1.25 = multiplying

NOTE: Smart UPS SC is called as the Back-UPS hybrid UPS. It belongs to Smart UPS family but the output waveform remains as approximated sine wave and it does not have a smart slot.

For PFC compatible Smart-UPS, please follow hyper links below and select your country of your choice for available offers:
Smart UPS Line-interactive 
Smart UPS Online 
Smart UPS Ultra (only available on selected regions)

For more details, you may contact APC support team .

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range: