{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Is it possible to mute the Audible Alarms on the Back UPS CS Series

Issue:

It is Possible to mute Alarms on some of the Back UPS units but not on all.

The Back UPS CS units can be monitored and controlled with PowerChute Personal Edition.

It is Possible to Mute the Alarms on the international model Back UPS CS 650, but not on the CS 500 or the CS 350 Model range.

Note: It is not possible to mute the BK650EI alarms without the use of PowerChute Personal Edition software.


Product Line:

Back-UPS CS


Environment:

BK650EI, BK500EI, BK350EI


Cause / Resolution:


To mute the alarms open PowerChute Personal Edition, select ""Notification"" under the configuration menu and click on ""Disable Battery Backup alarms at all times"". See the screen shot in the attachment."

Schneider Electric Egypt and North East Africa

Attachment(s)

Disable Alarms in the BackUPS CS650.docDisable Alarms in the BackUPS CS650.doc [65.5 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: