{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Do I need to install Java before installing PowerChute Network Shutdown?

Issue:
Do I need to install Java before installing PowerChute Network Shutdown?

Product:
PowerChute Network Shutdown

Environment:
All supported OS

Cause:
Installation

Resolution:
If you go to http://www.apc.com/tools/download/ and choose Software Upgrades - PowerChute Network Shutdown from the drop-down list, PDF documents listing supported JREs can be found.

PowerChute Version 5.0
PowerChute installs AdoptOpenJDK 11.0.16.1 for all supported operating systems

PowerChute Version 4.4.1, 4.4.2, 4.4.3
PowerChute installs OpenJDK 15 for all supported operating systems

PowerChute Version 4.4
PowerChute installs OpenJDK 14 for all supported operating systems.

PowerChute Version 4.3
With all supported operating systems except HP-UX®, AIX, and Mac OS X, PowerChute installs OpenJDK 11.
To install PowerChute on HP-UX, AIX, and Mac OS X, a compatible JRE must already be installed on your system.
Solaris Sparc gives you the option of installing the bundled JRE, or specifying a JRE location.

PowerChute Version 3.x, and 4.0, 4.1, 4.2
With all supported operating systems except HP-UX, AIX, and Mac OS X, PowerChute gives you the option of installing a "private" JRE during installation.
However, this "private" version of the JRE, which is specifically for PowerChute, will take up about 100 MB of disk space. A PowerChute installation takes up about 6 MB of space if you have already installed a public JRE.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: