{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Video: What to do if the system is missing native shutdown battery options / How to restore HID UPS device driver.

Issue:
Missing native shutdown battery options in Windows

Product Line:
Back-UPS and Smart-UPS

Environment:
7, 8, 10, 2008, 2010, 2012, 2016, 2019, 2022

Cause:
When viewing Power Options (go to Control Panel - Power Options) you may find that the configurable battery shutdown options are missing / not available. This may be caused by the HID driver (Human Interface Device) being updated from HID UPS to APC UPS or APC Battery BackUPS.

Solution:
If you are no longer using PowerChute software and want to utilize native battery options, you may need to roll / revert the HID Driver to HID UPS.
The featured video explains how to revert / restore HID UPS Driver that will allow for the configuration of native battery shutdown option.
For information on how to configure 7, 8, 10, 2008, 2010, 2012, 2016, 2019, 2022 to safely shutdown without using APC's PowerChute software please review FAQ Configuring Microsoft Windows 7, 8, 10, & 11 Windows Server 2008, 2012, 2016, 2019, & 2022 to safely shutdown without using APC's PowerChute software.

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.