This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
INTERNAL
Issue:
How to wire an actuator for an Airflow unit.
Product Line:
All Airflow units.
Environment:
All Serial Numbers
Cause:
Install/Repair
Resolution:
How to wire an actuator for an Airflow unit.
Product Line:
All Airflow units.
Environment:
All Serial Numbers
Cause:
Install/Repair
Resolution:
The below schematic works for M400 & M800 actuators. The system needs a 30VA transformer for the new actuator. The actuator dipswitches need to be adjusted for Floating [24v open & 24v close] dipswitches 1 & 2 on and the rest off.
Manual Operation
There is a red manual operation handle on the actuator, see figure 2. When it is lowered, the motor stops. Then the actuator can be operated manually if the handle is turned.
Original Wiring
New Wiring
ATTENTION: Actuators are shipped with manual override lowered (MAN). For normal operating, the handle must be raised (AUTO).