{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: What does a flashing E on the ATV212 or ATV21 display (External Fault on the graphic keypad) mean?

Article available in these languages: Czech, Spanish

Issue:
What does a blinking E on the ATV21 or ATV212 display mean?
What does External Fault mean on the graphic keypad?

Product Line:
Altivar 21
ATV21
Altivar 212
ATV212
S-flex enclosed ATV21/ATV212

Environment:
All

Cause:
Flashing E on the display of the ATV21 or ATV212 drive.

Resolution:
The drive is in a faulted status, initiated by one of the following:
1) CMOd is set to 0 or 2, the drive is in remote mode and the keypad STOP button is pressed.  Since the drive is looking for a stop command from a logic input or serial communications, the STOP button is assigned to function as an E-STOP. (See page 87 in the ATV212 Programming Manual and attachment)

2) A logic input is assigned as External Fault, functions 11 or 45, and that logic input fault is activated.
Check the following parameters:
F111 - Terminal F logic input assignment (default = 2; run forward)
F112 - Terminal R logic input assignment (default = 6; preset speed)
F113 - Terminal RES logic input assignment (default = 10; fault reset)

To reset the fault, either cycle power to the drive or activate a logic input that is assign as Fault Reset, functions 10 or 55.


Video uses the ATV212 drive for demonstration purposes:


Schneider Electric Egypt and North East Africa

Attachment(s)
ATV212_Installation_manual_EN_S1A53832_03.pdf [5.67 MB]
FAQ 000070517.png [49.92 KB]
Video: What does a flashing E on the ATV212 or ATV21 display (External Fault on the graphic keypad) mean?

Article available in these languages: Czech, Spanish

Issue:
What does a blinking E on the ATV21 or ATV212 display mean?
What does External Fault mean on the graphic keypad?

Product Line:
Altivar 21
ATV21
Altivar 212
ATV212
S-flex enclosed ATV21/ATV212

Environment:
All

Cause:
Flashing E on the display of the ATV21 or ATV212 drive.

Resolution:
The drive is in a faulted status, initiated by one of the following:
1) CMOd is set to 0 or 2, the drive is in remote mode and the keypad STOP button is pressed.  Since the drive is looking for a stop command from a logic input or serial communications, the STOP button is assigned to function as an E-STOP. (See page 87 in the ATV212 Programming Manual and attachment)

2) A logic input is assigned as External Fault, functions 11 or 45, and that logic input fault is activated.
Check the following parameters:
F111 - Terminal F logic input assignment (default = 2; run forward)
F112 - Terminal R logic input assignment (default = 6; preset speed)
F113 - Terminal RES logic input assignment (default = 10; fault reset)
 

To reset the fault, either cycle power to the drive or activate a logic input that is assign as Fault Reset, functions 10 or 55.


Video uses the ATV212 drive for demonstration purposes:


 

Schneider Electric Egypt and North East Africa

Attachment(s)
ATV212_Installation_manual_EN_S1A53832_03.pdf [5.67 MB]
FAQ 000070517.png [49.92 KB]
Explore more
Range:
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
Explore more
Range:
move-arrow-top