{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are there baying brackets available for the NetShelter VX Seismic cabinets?
Issue:
A question is asked if it's possible to bay together NetShelter VX Seismic cabinets.

Product Line:
NetShelter VX Seismic

Environment:
All versions and date ranges.

Cause:
Customers may want to use baying brackets to enhance the seismic feature, or to help align rows of cabinets.

Resolution:
There are no baying brackets for the NetShelter VX Seismic cabinets.
The NetShelter VX Seismic cabinets are designed to be mounted to the floor in NEBS GR-63-CORE seismic installations, and baying brackets are not necessary. Baying brackets do not enhance the seismic feature of the cabinet.

Schneider Electric Egypt and North East Africa