Issue:
Communication options available for ATV212 and S-Flex 212 Drives
Product Line:
ATV212, ATV212 S-Flex
Cause:
Customers want to know what are the standard communications in the ATV212 and ATV212 S-Flex drive.
Resolution:
Modbus, Metasys N2, BACnet and Apogee P1 are all standard, and built into the ATV212 and S-Flex 212 drives.
A LonWorks Card (VW3A21212) is optional, and provides a four screw terminal block for connections. This board is installed in place of the standard control board that comes with the ATV212 drive. Adding this LonWorks option card will reduce your I/O count to 3 logic inputs, 1 analog input and 1 NO/NC relay.
Communication options available for ATV212 and S-Flex 212 Drives
Product Line:
ATV212, ATV212 S-Flex
Cause:
Customers want to know what are the standard communications in the ATV212 and ATV212 S-Flex drive.
Resolution:
Modbus, Metasys N2, BACnet and Apogee P1 are all standard, and built into the ATV212 and S-Flex 212 drives.
A LonWorks Card (VW3A21212) is optional, and provides a four screw terminal block for connections. This board is installed in place of the standard control board that comes with the ATV212 drive. Adding this LonWorks option card will reduce your I/O count to 3 logic inputs, 1 analog input and 1 NO/NC relay.
Released for:Schneider Electric Egypt and North East Africa