{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is there a way to get more torque out of the motor when running at lower speeds with an ATV312 drive?
Issue:
How to increase the torque out of a motor when running at lower speeds with an ATV312 drive

Product Line:
ATV312

Environment:
All

Cause:
More torque

Resolution:
First, verify that the motor data is correct in the drC menu.  Then set UFt to L.  In the SEt menu, increase UFr to provide higher torque output.


Schneider Electric Egypt and North East Africa