Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
How humidity threshold alarms are reported on an ACRP
Issue:
This document will describe how humidity threshold alarms are reported on an ACRP.
 
Product line:
ACRP5XX, ACRP1XX, Uniflair, Network Air FM, ACFM, IR40, InRoom
 
Environment:
All Product models, all serial numbers
 
Cause:
Units use dew point to calculate humidity
 
Resolution:
You may come across an ACRP not generating an alarm message when the Return Humidity is lower than the Threshold [figure 1].  Remember Humidity set points and thresholds are based on dew point.  It is possible to be under the RH% set point/threshold and not receive a humidity demand or warning.
Figure 1

Schneider Electric Egypt and North East Africa

Attachment(s)
ACRP Not Reporting Humidity Alarm Threshold Violations rev. 20121207.doc [814 KB]