This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Issue:
What are the length of the power cords of an ACSC.
Product line:
ACSC100, ACSC103.
Environment:
All Product models, all serial numbers.
Cause:
Resolution:
ACSC Power cord lengths
•60 Hz unit – 5.5 Feet (1.7 m)
•50 Hz unit – 12 Feet (3.6 m)
Released for:Schneider Electric Egypt and North East Africa