Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
General principles and guidelines on air intakes and outlets

Issue:

General principles and guidelines on air intakes and outlets

 

Product line:

All Air removal equipment

 

Environment:

All Product models, all serial numbers

 

Cause:

Pressure issues that can occur from improper balance

 

Resolution:

Air Intakes and Outlets

Ventilation systems - air intakes and outlets and rules of thumbs

 

 

Intakes

  • Intakes should be at least 0.15 m (0.5 ft) above the terrain.  In areas with traffic the intake should be at least 5 m (16 ft) above the terrain.
  • The distance between intake, firewalls, and surrounding buildings must be according the rules of the local authorities.
  • Short cutting intake air with used outlet air must be avoided.
  • An air intake should be located in a position where the wind influence on the pressure conditions within the system is limited.
  • Air velocities in the intake openings should not exceed 2.5 m/s (~ 500 ft/min)

Outlets

  • Outlets should go direct out in unrestricted area.
  • Short cuts with intake air, window openings and residence areas must be avoided.
  • The distance between outlet, firewalls and surrounding buildings must be according the rules of the local authorities.
  • An air outlet should be located in a position where the wind influence on the pressure conditions within the system is limited.
  • The air velocity through the outlet should not exceed 3 - 15 m/s (~ 500 - 3000 ft/min).

 

 

 

 

Schneider Electric Egypt and North East Africa

Attachment(s)
K-B - Air Intakes and Outlets.doc [25.5 KB]
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more