Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the suitable Minimum load percentage required for ACB to work proberly (micrologic trip unit) ?
It is 20%, i.e. you need to have 800A load atleast for a 4000A ACB, for the ACB to work properly (i.e. to have Micrologic display illumination).

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range: