{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to program the ATV31 or ATV312 analog output for 4-20mA, 0-20mA or 0-10 V signal?
Issue:
ATV31/ATV312 analog output configuration for 4-20mA, 0-20mA or 0-10 V signal

Product line:
ATV31, ATV312

Environment:
All range All serial number

Cause:
How to get a feedback signal form the ATV312?

Resolution:
Steps to program the analog output of the ATV31 or ATV312
1). Press the enter key to REF
2). Turn dial (ATV312) or press the down arrow (ATV31) to I-O menu Press enter
3). Turn dial or press the down arrow to AO1t Press enter
The following selections are available, choose one and press enter
a). 0A – Current – 0-20mA configuration (use terminal AOC)
b). 04 – Current – 4-20mA configuration (use terminal AOC)
c). 10U – Current – 0-10 V configuration (use terminal AOV)
4). Press esc to AO1t
5). Turn dial to d0
The following selections are available for the analog output, choose one and press enter
a). OCr (motor current) – 20 mA or 10 V corresponds to twice nominal drive current
b). OFr (Motor Frequency) – 20 mA or 10 V corresponds to the maximum frequency(tFr)
c). Otr (Motor Torque) - 20 mA or 10 V corresponds to twice nominal motor torque
d). OPr (Power supplied) – Power supplied by the drive, 20 mA or 10 V corresponds to twice the drive power.
6). Esc out of all menus. Drive is ready to run once the analog signal wiring is connected.

Schneider Electric Egypt and North East Africa