This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Issue:
The article addresses the question of, what is the input voltage required for the InRow ACRD100/200? Is a power cord supplied with the unit?
Product line:
ACRD100.
Environment:
All versions.
Cause:
Install.
Resolution:
The InRow RD unit uses a single phase 208V/60Hz input in NAM and a 230V/50Hz input in the rest of the world. Is a power cord supplied with the unit? No
The article addresses the question of, what is the input voltage required for the InRow ACRD100/200? Is a power cord supplied with the unit?
Product line:
ACRD100.
Environment:
All versions.
Cause:
Install.
Resolution:
The InRow RD unit uses a single phase 208V/60Hz input in NAM and a 230V/50Hz input in the rest of the world. Is a power cord supplied with the unit? No