Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the function of the " ASY " potentiometer in the RM35 relays ?
The " ASY" potentiometer is concerned with the asymmetry function between phases. You can set the percentage between 5% and 15 % of the default voltage value. If the voltage on one phase falls under the specified value, the relay will give a signal.
The difference between this function and the under voltage function is that the under voltage has a higher range. It considers the voltage as a total but it doesn't consider the asymmetry between phase waves.

Schneider Electric Egypt and North East Africa