{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.

Is there a thermal overload relay in Schneider offer with tripping class 30 ?

Schneider Electric does not have Trip class 30 thermal overload relays.

If the application is less than 15KW , you can use the Tesys U with the multifunction control unit type LUCM where you have an option of trip class selection from 5 to 30.

If the application is greater than 15KW , you can use the Tesys T . It also provides you the option of selection of trip class from 5-30.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: