Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the short circuit withstand rating ( Isc ) for ( GV2G445 ) ?
This bus bar does not have a conditional short-circuit rating. The short-circuit current withstand is compatible with the breaking capacity of motor protection circuit breakers GV2** with which the bus bar is used.
So the Isc of the GV2G** depends on the GV2ME/P energized ratings. You can use a circuit breaker or fuses in upstream of the GV2G445 for a short circuit value up to 11KA as the permissible peak current of GV2G445 is 11KA. ( See attachment).

Schneider Electric Egypt and North East Africa

Attachment(s)
GV.pdf [36.14 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: