This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Issue:
This article contains the manuals for Carrier 30RA010-055 AquaSnap® Air-Cooled Chillers with ComfortLink™ Controls 50/60 Hz
Product line:
Carrier 30RA010-055.
Environment:
All Serial Numbers.
Cause:
Controls, Start-Up, Operation, Service, and Troubleshooting.
Resolution:
See attached manuals