{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How is the ATV212 set for HMI controls for both RUN/STOP and speed reference?

Article available in these languages: Spanish

Issue:
How is the ATV212 set for HMI controls for both RUN/STOP and speed reference?

Product Line:
Altivar 212

Environment:
All models

Cause:
Control for VFD to be from the HMI

Resolution:
There are several options.
1) Put the VFD in Local Mode by pressing the LOC/REM button on the integral keypad, or the F4 button on the remote keypad.  Indicators for Local Mode are the green LED is ON for LOC/REM, or LOC is displayed above the F1 button.
2) Keep the VFD in Remote Mode and set CMOd=1 and FMOd=3

Both of these options apply for integral keypad or remote keypad control.

Schneider Electric Egypt and North East Africa