{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.

For the ATS controllers ( UA and BA ), can both of them be used with ACB master pact range of NW and NT or not ?

The UA and BA are two types of ATS sequence controller. It is used with the following ranges:
- MCCB of type NSX and NS
- ACB of types NW and NT

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: