Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
ACOA5XX cooling failure
Issue:
This dcoument describes the issues that can cause an ACOA5XX cooling failure.
Product line:
ACOA5XX.
Environment:
All Serial Numbers.
Cause:
Supply Air Temperature> 90 F and Cooling Output < 4 kW.
Resolution:
Supply Air Temperature> 90 F and Cooling Output < 4 kW
OA will shut down
OA will restart after 5 Min
If conditions still exists after 60 seconds OA will shut down.
tf = 300oF* sec/ tsup - 90oF
Where
Tsup is the average supply air temperature in oF
Released for:Schneider Electric Egypt and North East Africa
Attachment(s)
Explore more
Range:
Explore more
Range: