{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: How is the ATV212 set up for a run permissive logic input?
Issue:
Setting up the  ATV212  for a run permissive

Product Line:
ATV212 S-Flex212

Environment:
All models and serial numbers

Cause:
N/A

Resolution:
Wire a dry contact to P24 and a logic input (F, R, or RES).  Program F110 = 0 to remove the always active run permissive.  Then set the logic input = 1 to assign run permissive to it (F111=1, F112=1, or F113=1).  When the remote contact is closed, the drive is permitted to run and is ready for a run command.

Schneider Electric Egypt and North East Africa