Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the short time withstand current ( Icw ) for MCCB of type NSX ?
We have no Icw (rated short-time withstand current) values for the NSX up to 630A. These devices have an utilization category A according to IEC 60947-2 standards which means that they are not specifically intended for selectivity under short-circuit conditions with respect to other short-circuit protective devices in series on the load side. They are without an intentional short-time delay provided for selectivity under short-circuit conditions and therefore without a short-time withstand current rating. According to IEC 60947-2 Icw exists only for category B circuit breakers and switch disconnectors.
 

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: