Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the main difference between Tesys "U" and Tesys "T" ?
- Tesys "U" is a motor starter used instead of the conventional starting methods (Motor CB + Contactor + Thermal Overload) and it provides full coordination performance and it is used up to 15 KW (much more better than type 1 and type 2 coordinations)
- Tesys "T" is a Motor protection relay that supports different types of communication (profibus - Modus - Ethernet ...) and is used for motor protection of the LV level from under & over voltage, frequency changes, reversing power direction and many other LV protection functions.
- Tesys "T" is a Motor protection relay that supports different types of communication (profibus - Modus - Ethernet ...) and is used for motor protection of the LV level from under & over voltage, frequency changes, reversing power direction and many other LV protection functions.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: