This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Issue:
This document contains all technical data in the ACSC100 Tech Data Manual.
Product line:
ACSC100, ACSC101.
Environment:
All Serial Numbers.
Cause:
Tech Data Manual.
Resolution:
See file below
Additonal spec's:
Evaporator Fan Speed | Standard Volumetric Air Flow Rate |
% | SCFM |
100 | 1190 |
90 | 1090 |
80 | 960 |
70 | 880 |
60 | 820 |
Fan Speed % | A Weighted Sound Pressure dBA in a 10' X 10' X 10' room at 5 ft distance | ||||
EvF100% ; CondF100% | 82.2 | ||||
EvF90% ; CondF100% | 81 | ||||
EvF80% ; CondF100% | 80.5 | ||||
EvF60% ; CondF80% | 78.1 |