This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Issue:
ACRD200 Internal Water Volume
Product line:
ACRD200, ACRD201
Environment:
Cause:
Inrow Water Cooled Units Internal Volumes
Resolution:
ACRD20x 0.8 Gallons 3 Liters 10GPM
Note: working system pressure may not exceed 300 psi
Additional Spec's: