{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Oil Type for Different Types of Refrigerant

Article available in these languages: Spanish

Issue:
Oil Type for Different Types of Refrigerant

Product line:
All AC DX Units

Environment:
All versions/serials

Cause:
Oil Maintenance

Resolution:
Below is a list of the different oil types for the different refrigerants in our units. Always check the compressor manufacture's recommendations for oil on any other type of cooling unit.

R 12                 Use Mineral Oil or Alkyl Benzene Oil

R 22                 Use Mineral Oil, Mixing of POE is acceptable however it is preferred to use the oil that the original charge used.  Units: AX, CM, CC T, DT, TC, FM, ACPA4000, AP7003

R134A            Use POE oil      Units: RDU but no oil needed for this unit on startup.

R407C            Use POE oil     Units: ACRP, ACRD5xx, Stulz

R410A            Use PVE oil      Units: ACRD1XX, ACRD2XX, ACRD3XX,ACRD60XX, ACRD6XXP ACSC, Uniflair, ACPSC, Ecobreeze

POE oil recommendations 150, 160 Viscosity.

Copelands POE oil Part# 998-E022-01

Ultra 32-3MAF

PVE oil recommendations 320HV or FVC68D or better yet Danfos 120Z5034

Schneider-Electric Sku for POE oil: 0J-9099

Note: Prior to adding any oil to a system a leak check should be completed and a proper acid test completed.

Schneider Electric Egypt and North East Africa