Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
I have " NST " error code on the ATV312 display and it doesn't want to run.
" NST " stands for freewheel stop mode.This means that the stop signal into one of the assigned logic inputs is cut ( since the freewheel stop function is active at " 0 " ).  So, you have to check the wiring.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: