This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Type 1 & 2 surge arresters are installed directly under the incoming breaker. We use Type 1 when there is a lightning bolt installed on the building roof. When there's not, we use Type 2.
Type 3 is installed in parallel with the sensitive loads ( Computers, printers...etc. )
Type 3 is installed in parallel with the sensitive loads ( Computers, printers...etc. )
Released for: Schneider Electric Egypt and North East Africa